Codewarrior rename file?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior rename file?

ソリューションへジャンプ
1,647件の閲覧回数
eliezeroc
Contributor III

Hello. How do I rename files with extension abs, args, s19 who are in FLASH CodeWarrior folder? I took the project_01 to make project_01 actually copied and pasted, there clicked the right button on the project and rename, but the FLASH folder files were not renomedos. Is there any way to rename this file without creating a new project?

I already try renaming the files by renaming building but when they go back to the previous name. Grateful.

ラベル(1)
1 解決策
1,510件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

the file name used for the output is specified as artifact name in the project properties:

pastedImage_0.png

I hope this helps,

Erich

元の投稿で解決策を見る

1 返信
1,510件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

the file name used for the output is specified as artifact name in the project properties:

pastedImage_0.png

I hope this helps,

Erich