Codewarrior rename file?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior rename file?

Jump to solution
1,647 Views
eliezeroc
Contributor III

Hello. How do I rename files with extension abs, args, s19 who are in FLASH CodeWarrior folder? I took the project_01 to make project_01 actually copied and pasted, there clicked the right button on the project and rename, but the FLASH folder files were not renomedos. Is there any way to rename this file without creating a new project?

I already try renaming the files by renaming building but when they go back to the previous name. Grateful.

Labels (1)
1 Solution
1,510 Views
BlackNight
NXP Employee
NXP Employee

Hello,

the file name used for the output is specified as artifact name in the project properties:

pastedImage_0.png

I hope this helps,

Erich

View solution in original post

1 Reply
1,510 Views
BlackNight
NXP Employee
NXP Employee

Hello,

the file name used for the output is specified as artifact name in the project properties:

pastedImage_0.png

I hope this helps,

Erich