Codewarrior Eclipse and S12(X) Family

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior Eclipse and S12(X) Family

2,678 Views
ZdenoQC
Contributor III

Hi there,

 

I was previously working with the s08dz60 uC and the Codewarrior classic IDE. Now that I have ported my project to Codewarrior Eclipse, I find it way more better than the Classic. But Right now I work with the S12G family of uC and I'm stock with the classic IDE.

 

My question:

Is there any plan to integrate the S12(X) family of uC in Codewarrior Eclipse?

 

Thanks

 

William

Labels (1)
0 Kudos
Reply
3 Replies

2,455 Views
BlackNight
NXP Employee
NXP Employee

You could use the S12 (or S08) tools from Eclipse. The simplest way is to have a make file and call the build tools that way.

And the debugger can be called as exernal debugger as in CodeWarrior.

Erich

0 Kudos
Reply

2,455 Views
ZdenoQC
Contributor III

I will try this.

Thanks Erich!

0 Kudos
Reply

2,455 Views
PatrickMenter
NXP Employee
NXP Employee

William,

There are no plans to port S12G support to the CW for MCU in Eclipse.

Patrick Menter

0 Kudos
Reply