Codewarrior Eclipse and S12(X) Family

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrior Eclipse and S12(X) Family

2,700 次查看
ZdenoQC
Contributor III

Hi there,

 

I was previously working with the s08dz60 uC and the Codewarrior classic IDE. Now that I have ported my project to Codewarrior Eclipse, I find it way more better than the Classic. But Right now I work with the S12G family of uC and I'm stock with the classic IDE.

 

My question:

Is there any plan to integrate the S12(X) family of uC in Codewarrior Eclipse?

 

Thanks

 

William

标签 (1)
0 项奖励
回复
3 回复数

2,477 次查看
BlackNight
NXP Employee
NXP Employee

You could use the S12 (or S08) tools from Eclipse. The simplest way is to have a make file and call the build tools that way.

And the debugger can be called as exernal debugger as in CodeWarrior.

Erich

0 项奖励
回复

2,477 次查看
ZdenoQC
Contributor III

I will try this.

Thanks Erich!

0 项奖励
回复

2,477 次查看
PatrickMenter
NXP Employee
NXP Employee

William,

There are no plans to port S12G support to the CW for MCU in Eclipse.

Patrick Menter

0 项奖励
回复