Codewarrior 8.7 MPC566EVB dbug monitor restore

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior 8.7 MPC566EVB dbug monitor restore

2,046件の閲覧回数
leizhihualqytvw
Contributor I


Hello

 

I am using MPC566EVB for the project, but I can't get the dBug monitor message on the terminal when power on the board. I have downloaded codewarrior PowerPC 5xx V8.7 and want to use it to restore the dbug ROM software for the board,however i can debug and run the "Welcom to Codewarrior" demo, but i havn't the dBug software for the board,Would you help provide the dbug software and tell me how to restore it with codewarrior? thanks!

 

LZH

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,886件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

I've found the dBug monitor image here:

http://www.axman.com/sites/default/files/mpc566evb_dBUG%20monitor%20S%20record_v1.zip 

As far as I know CodeWarrior for MPC5xx v8.7 includes flash programmer which you can use to program dBug ROMmonitor srecord.

Unfortunately I don't have a board to test.

Hope it helps.

Stan

0 件の賞賛
返信

1,886件の閲覧回数
leizhihualqytvw
Contributor I

Hi Stan,

I download the dBug ROMmonitor srecord file from AXMAN website,and to programm the image with Codewarrior MPC5xx v8.7 Flash Programmer,but the programmer can't burn the srecord and show--" 0 Bytes Programmed, Check Restricted Address Range" and more details infor as below and attach picture,however i can erase the all external flash and burn the "Welcom to CodeWarrior!" demo image(rom.elf),but I can't successfully burn this dBug ROMmonitor srecodd image file,Would you help give us some suggestion to close the issue?thanks for your support!

LZH

1.JPG

=====================================================================================================================
======================================================================
=== Target Configuration Settings
=== Connection:       CodeWarrior USB TAP
=== Target Processor: 566
=== Target Init File: C:\Program Files\Freescale\CodeWarrior EPPC 5xx V8.7\PowerPC_EABI_Support\Initialization_Files\5xx\MPC566EVB_MPC565_MPC566_init.cfg
======================================================================
Connecting......Connected


======================================================================
=== Execute: Erase
=== Timestamp:  Thu Mar  2 19:14:22 2017
=== Flash Device:         AM29BDD160GT
=== Flash Organization:   512Kx32x1
=== Flash Mem Start Addr: 0xFFE00000
=== Flash Mem End Addr:   0xFFFFFFFF
======================================================================
Using Algorithm: amd32x1.elf
 
Informing other connection clients that the target is being 'clobbered'.
Loading Flash Device Driver at: 0x00C02000
Flash Driver Buffer is at:      0x00C03DB0
Flash Driver Buffer Size is:    0x0005E250
Done

Initialization Command Succeeded
Erasing Sector 0xFFE00000 to 0xFFE01FFF ...
Erasing Sector 0xFFE02000 to 0xFFE03FFF ...
Erasing Sector 0xFFE04000 to 0xFFE05FFF ...
Erasing Sector 0xFFE06000 to 0xFFE07FFF ...
Erasing Sector 0xFFE08000 to 0xFFE09FFF ...
Erasing Sector 0xFFE0A000 to 0xFFE0BFFF ...
Erasing Sector 0xFFE0C000 to 0xFFE0DFFF ...
Erasing Sector 0xFFE0E000 to 0xFFE0FFFF ...
Erasing Sector 0xFFE10000 to 0xFFE1FFFF ...
Erasing Sector 0xFFE20000 to 0xFFE2FFFF ...
Erasing Sector 0xFFE30000 to 0xFFE3FFFF ...
Erasing Sector 0xFFE40000 to 0xFFE4FFFF ...
Erasing Sector 0xFFE50000 to 0xFFE5FFFF ...
Erasing Sector 0xFFE60000 to 0xFFE6FFFF ...
Erasing Sector 0xFFE70000 to 0xFFE7FFFF ...
Erasing Sector 0xFFE80000 to 0xFFE8FFFF ...
Erasing Sector 0xFFE90000 to 0xFFE9FFFF ...
Erasing Sector 0xFFEA0000 to 0xFFEAFFFF ...
Erasing Sector 0xFFEB0000 to 0xFFEBFFFF ...
Erasing Sector 0xFFEC0000 to 0xFFECFFFF ...
Erasing Sector 0xFFED0000 to 0xFFEDFFFF ...
Erasing Sector 0xFFEE0000 to 0xFFEEFFFF ...
Erasing Sector 0xFFEF0000 to 0xFFEFFFFF ...
Erasing Sector 0xFFF00000 to 0xFFF0FFFF ...
Erasing Sector 0xFFF10000 to 0xFFF1FFFF ...
Erasing Sector 0xFFF20000 to 0xFFF2FFFF ...
Erasing Sector 0xFFF30000 to 0xFFF3FFFF ...
Erasing Sector 0xFFF40000 to 0xFFF4FFFF ...
Erasing Sector 0xFFF50000 to 0xFFF5FFFF ...
Erasing Sector 0xFFF60000 to 0xFFF6FFFF ...
Erasing Sector 0xFFF70000 to 0xFFF7FFFF ...
Erasing Sector 0xFFF80000 to 0xFFF8FFFF ...
Erasing Sector 0xFFF90000 to 0xFFF9FFFF ...
Erasing Sector 0xFFFA0000 to 0xFFFAFFFF ...
Erasing Sector 0xFFFB0000 to 0xFFFBFFFF ...
Erasing Sector 0xFFFC0000 to 0xFFFCFFFF ...
Erasing Sector 0xFFFD0000 to 0xFFFDFFFF ...
Erasing Sector 0xFFFE0000 to 0xFFFEFFFF ...
Erasing Sector 0xFFFF0000 to 0xFFFF1FFF ...
Erasing Sector 0xFFFF2000 to 0xFFFF3FFF ...
Erasing Sector 0xFFFF4000 to 0xFFFF5FFF ...
Erasing Sector 0xFFFF6000 to 0xFFFF7FFF ...
Erasing Sector 0xFFFF8000 to 0xFFFF9FFF ...
Erasing Sector 0xFFFFA000 to 0xFFFFBFFF ...
Erasing Sector 0xFFFFC000 to 0xFFFFDFFF ...
Erasing Sector 0xFFFFE000 to 0xFFFFFFFF ... Done

Erase Command Succeeded
Timestamp:  Thu Mar  2 19:14:49 2017
: No Error

======================================================================
=== Execute: Program
=== Timestamp:  Thu Mar  2 19:15:02 2017
=== Flash Device:         AM29BDD160GT
=== Flash Organization:   512Kx32x1
=== Flash Mem Start Addr: 0xFFE00000
=== Flash Mem End Addr:   0xFFFFFFFF
======================================================================
Using restricted address range 0xFFE00000 to 0xFFFFFFFF

Using Algorithm: amd32x1.elf
 
Informing other connection clients that the target is being 'clobbered'.
Loading Flash Device Driver at: 0x00C02000
Flash Driver Buffer is at:      0x00C03DB0
Flash Driver Buffer Size is:    0x0005E250
Done

Initialization Command Succeeded
Programming file D:\Downloads\mpc566evb_dBUG monitor S record_v1\mpc566evb_flash_v1.s19
Trying auto-detect...
Auto-detection is successful.
  File is of type Motorola S-Record Format.

Programmed total of 0x00000000 bytes

Timestamp:  Thu Mar  2 19:15:04 2017
: No Error

======================================================================
=== Target Configuration Settings
=== Connection:       CodeWarrior USB TAP
=== Target Processor: 566
=== Target Init File: C:\Program Files\Freescale\CodeWarrior EPPC 5xx V8.7\PowerPC_EABI_Support\Initialization_Files\5xx\MPC566EVB_MPC565_MPC566_init.cfg
======================================================================
Connecting......Connected


======================================================================
=== Execute: Program
=== Timestamp:  Thu Mar  2 19:16:27 2017
=== Flash Device:         AM29BDD160GT
=== Flash Organization:   512Kx32x1
=== Flash Mem Start Addr: 0xFFE00000
=== Flash Mem End Addr:   0xFFFFFFFF
======================================================================
Using restricted address range 0xFFE00000 to 0xFFFFFFFF

Using Algorithm: amd32x1.elf
 
Informing other connection clients that the target is being 'clobbered'.
Loading Flash Device Driver at: 0x00C02000
Flash Driver Buffer is at:      0x00C03DB0
Flash Driver Buffer Size is:    0x0005E250
Done

Initialization Command Succeeded
Programming file D:\Downloads\mpc566evb_dBUG monitor S record_v1\mpc566evb_flash_v1.s19

Programmed total of 0x00000000 bytes

Timestamp:  Thu Mar  2 19:16:29 2017

==================================================================================================

0 件の賞賛
返信