Codewarrier reference applications(Non OS) for MPC8306 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrier reference applications(Non OS) for MPC8306 processor

1,891件の閲覧回数
nthiru28
Contributor I

Hi All,

 

I'm trying to develop standalone application for MPC8306 based board, which doesn't support any Operating system.

 

Please can anyone suggest me the proper document to start learning about Register Configuration in codewarrior and reference applications except hello world which is default with Codewarrior. ?

 

Regards,

Thiru N

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,773件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello Thiru N,

If you are using CW for PA 10, you could find some bared board example in the CW installation directory:

D:\Freescale\CW_PA_v10.5.1\PA\CodeWarrior_Examples\Bareboard_Examples

If you are using CW for PowerQUICC(Classic IDE), you could also find CodeWarrior example in the CW installation directory:

C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\(CodeWarrior_Examples)

For the "Register Configuration in codewarrior", I am not sure what you mean, please elaorate, thanks.

Regards

Lunmin

0 件の賞賛
返信

1,773件の閲覧回数
nthiru28
Contributor I

Hi Lunmin,

Thanks for your response.

I'm using Code-warrior v8.8 and also using Freescale TAP for programing.

Can you please specify the example application which works for MPC8308

Registry configuration in the sense, the processor initial configuration

and *.lcf file.

Regards,

Thiru N

*For the "Register Configuration in codewarrior", I am not sure what you

mean, please elaorate,*

I'm expecting the configuration file of MPC8308 related to bare code of

On Mon, May 9, 2016 at 10:44 AM, lunminliang <[email protected]>

0 件の賞賛
返信