CodeWorrior 5.1 compatibility with Windows 10 Pro 64bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWorrior 5.1 compatibility with Windows 10 Pro 64bit

3,780 Views
wei_w_he
Contributor IV

Dear Officer,

Due to legacy issue, we need to use CW5.1, and our PC is using Windows 10 Pro 64bit now, Can CW5.1 being still supported fro Win10 Pro 64 bit system? Any patch required?

How about CW5.2?

Thanks and best regards

He Wei

7 Replies

3,562 Views
wei_w_he
Contributor IV

Dear Jun Zhang,

I downloaded CW5.2 specific version CWS12v5.2_Win_b151201_se.exe, it seems working fine on Win10, but it doesn't support:

S12VR serials e.g. it doesn't support MC9S12VR48MLF, - it is used for our project.

Can you advise any way to add in these device support in CW5.2 specific version?

Thanks and best regards

He Wei

0 Kudos
Reply

3,562 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

He Wei

 We have VR patch for CW5.1. See if this document can help you.

How to install missing device to CodeWarrior for HCS12 v5.2 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,562 Views
wei_w_he
Contributor IV

Dear Jun Zhang,

It really helps and thanks you very much. Just one question: I can see all S12VR serials are added when try to "Create new project" (including S12VR16, S12VR32, S12VR48 and S12VR64),  but when running a project and under " Device and connection", I can only see S12VR64, is this normal? and S12VR64 can be commonly used for S12VR48 and SV12VR32 for debugging connection?

Thanks and best regards

He Wei

0 Kudos
Reply

3,562 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You said "when running a project and under " Device and connection", I can only see S12VR64 "

Can you please send me a screenshot of it?

0 Kudos
Reply

3,562 Views
wei_w_he
Contributor IV

Dear Jun Zhang

pastedImage_1.png

I can see all the VR serials during create new project.

pastedImage_2.png

0 Kudos
Reply

3,562 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

He Wei

I checked my CW5.2, I don't have this problem.

I also checked CW5.2 can support MC9S12VR48 naturally.

This is CW5.2 device support list:
> - MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96
> - MC9S12G128, MC9S12G96
> - MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64
> - MC9S12GN16, MC9S12GN32
> - MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128
> - MC9S12XEP100, MC9S12XEP768
> - MC9S12XEQ384, MC9S12XEQ512
> - MC9S12XET256
> - MC9S12XS128, MC9S12XS256, MC9S12XS64
> - MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64

Please reinstall CW5.2 or install it on another PC then test again.

 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,562 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi He Wei 

CW5.1 itself doesn't support win10. 

If you use P&E debug/programming tool, you can workaround the problem with P&E patch:

PEmicro | Experts in Embedded tools for Flash Programming and Development 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply