CodeWarriorUSBTAP驱动问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarriorUSBTAP驱动问题

7,697 Views
zzzc
Contributor I

问题如图,驱动工作。

0 Kudos
Reply
5 Replies

7,632 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you give detailed information, for example the DSC part number, the CodeWarrior for DSP56800E ver8.3 or CodeWarrior for MCU ver11.x?

BR

XiangJun Rong

0 Kudos
Reply

7,618 Views
zzzc
Contributor I
不好意思,我是第一次使用,我不知道怎么去寻找你上面所说的信息
0 Kudos
Reply

7,611 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the FlashProgrammer tools can not run on the Win 10 OS, and it has not updated for a long time.

I suggest you use CodeWarrior for MCU ver11.x tools to download application code to flash.

This is the website of CodeWarrior for MCU ver11.x tools:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

 

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

7,606 Views
zzzc
Contributor I
不是的,他在别人的win10上是可以使用的,然后我在虚拟机上添加win10和win7都不可以。我自己的电脑win11,我的截图就是我在win11上的截图,我怀疑有没有可能是安装包有问题。不知道您那边能提供新的安装包吗
0 Kudos
Reply

7,597 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

您用哪种芯片呢? 举个例子DSP56F805, MC56F8323, MC56F84789?

BR

XiangJun Rong

0 Kudos
Reply