CodeWarrior11.1 make a library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior11.1 make a library

3,428件の閲覧回数
zhipeng
Contributor III

请教一下,CodeWarrior11.1,如何生成库,没有找到这个版本的教程

版本如下:

Installed Products:
- CodeWarrior for MCU
Version: 11.1

 

I use Codewarrior 11.1 and would like to make a common library .

How can i make library files with CodeWarrior 11.1.

No tutorials found for this version

Installed Products:
- CodeWarrior for MCU
Version: 11.1

 

 

0 件の賞賛
返信
5 返答(返信)

3,414件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

select File -> New -> Bareboard Project

Add your project name and click on Next, select MPC5646C and select Library project like this:

lukaszadrapa_0-1672834447833.pnglukaszadrapa_0-1672834447833.png

And that's it.

lukaszadrapa_1-1672834557979.pnglukaszadrapa_1-1672834557979.png

When you build the project, *.a library file is created.

Regards,

Lukas

0 件の賞賛
返信

3,388件の閲覧回数
zhipeng
Contributor III

Thank you very much for your assistance, we tried the test code according to this process and it worked, but our official code is larger and many errors are reported, we are still debugging.
Also, can you please tell me if it's okay to choose default for this?

zhipeng_0-1673433232609.pngzhipeng_0-1673433232609.png

 

0 件の賞賛
返信

3,381件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

You should use the same configuration for library and for your project where the library will be used.

For example, if a library is compiled for VLE instruction set, it won't work in BOOKE project, of course...

Regards,

Lukas

0 件の賞賛
返信

3,422件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

请告知您的芯片型号。

谢谢,

Jun Zhang

0 件の賞賛
返信

3,418件の閲覧回数
zhipeng
Contributor III

您好,感谢答复,型号是SPC5646CCVLU1。谢谢

0 件の賞賛
返信