CodeWarrior support for QorIQ T1024 Processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior support for QorIQ T1024 Processor

1,426件の閲覧回数
manjularajesh
Contributor II

We are using CodeWarrior Development Studio for Power Architecture(version 10.3.3, Build Id:131024), Currently we started our design using T1024 processor this Codewarrior version is not supporting T1024RDB. Can we upgrade to higher version for T1024 support?? What is the procedure to upgrade, please provide web-links of the same.

 

regards,

manjula

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,318件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

I've checked with the last version CW for PA V10.5.

This version is is supporting the T1024RDB board.

How to get it ?

You can download the tool via our web site:

    CodeWarrior Dev Tools for Power Architecture|Freescale

For the license file, it depends of your registration.

I recommend you to check your registration to see if you can upgrade it for free or not.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信