CodeWarrior starting problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior starting problem

1,985 Views
catalin_hirceag
Contributor I

I just finished instaling codewarrior and tried adding a demo but i got this error: pastedImage_1.png

Is there any aditional software or plugins that i need too install?

Also i tried creating a new Bareboard Project, but cant fiind the micro i am using in that list.

The micro i use is a S9KEAZ128AMLK.

Thank You.

0 Kudos
Reply
2 Replies

1,875 Views
catalin_hirceag
Contributor I

Well i had some plugins missing and didn't see the micro in the list, but after I installed them it works.

Thank you anyway.

0 Kudos
Reply

1,876 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi [email protected]‌,

To create a new project using the KEA select the bare board option selecting File Tab ->New->Bareboard project

pastedImage_1.png

For the KEA family, these are under the Kinetis E series:

pastedImage_3.png

I hope this helps you.

Best Regards,

Alexis Andalon 

0 Kudos
Reply