CodeWarrior for WCT1012

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for WCT1012

2,817 Views
samuel_xp_zhang
Contributor I

I download and install CodeWarrior Version 10.6, I use it to open WCT1012 (Wireless Charging Transmitter MCU) example project, but it comes the error message:

 

Unknown target type: com.freescale.cw.system.dsc.MWCT1x1x.MWCT1012

 

How can I fix it?

 

Regards

Sam

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,498 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Samuel,

I would recommend you to download CodeWarrior 10.6.4 which is the latest release, it already comes support for the WCT1012 devices:

pastedImage_2.png

You can download it from this page:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,498 Views
samuel_xp_zhang
Contributor I

Hi Carlos,

After install CW10.6.4, I  fix this problem.

But I build a project for MWCT1012, no Processor Expert supported, is that right? or I need install Processor Expert for it?

Regards

Sam

0 Kudos
Reply

2,498 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Samuel,

You are correct, the MWCT1012 devices are not supported by Processor Expert.

Best Regards!

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply