CodeWarrior for WCT1012

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for WCT1012

2,836件の閲覧回数
samuel_xp_zhang
Contributor I

I download and install CodeWarrior Version 10.6, I use it to open WCT1012 (Wireless Charging Transmitter MCU) example project, but it comes the error message:

 

Unknown target type: com.freescale.cw.system.dsc.MWCT1x1x.MWCT1012

 

How can I fix it?

 

Regards

Sam

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,517件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Samuel,

I would recommend you to download CodeWarrior 10.6.4 which is the latest release, it already comes support for the WCT1012 devices:

pastedImage_2.png

You can download it from this page:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,517件の閲覧回数
samuel_xp_zhang
Contributor I

Hi Carlos,

After install CW10.6.4, I  fix this problem.

But I build a project for MWCT1012, no Processor Expert supported, is that right? or I need install Processor Expert for it?

Regards

Sam

0 件の賞賛
返信

2,517件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Samuel,

You are correct, the MWCT1012 devices are not supported by Processor Expert.

Best Regards!

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信