CodeWarrior for MCU v10.7 - MC56F8135 - USB TAP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for MCU v10.7 - MC56F8135 - USB TAP

Jump to solution
3,198 Views
edouardmalot
Contributor II

Hi,

I would like to use CodeWarrior 10.7 on an 56F8135 MCU with an USB TAP (debugger) 

I have done setup.bat in "C:\Freescale\CW MCU v10.7\MCU\ccs\drivers\usb" and my device seems to be correctly detected : 

pastedImage_1.png

In CodeWarrior in create a "new workspace", "new MCU project", and select MC56F8135 :

pastedImage_5.png

For programmer I choose "Freescale USB TAP"

pastedImage_6.png

After the project creation, the compilation work well.

If I try to program the device with "Flash file to target" window :

 1) I need a "Flash configuration file" but the file "MC56F8135.xml" does'nt exist so I use the "MC56F8335.xml" instead :

pastedImage_15.png

     (In Connection, Edit, options are as below) 

pastedImage_13.png

2) When I click to "Erase Whole Device" I get the error message below :

pastedImage_16.png

On the USB TAP, TX/RX led blink in green and Run/Pause led is OFF.

Does this issue is due to bad Flash configuration file" (MC56F8335.xml instead of MC56F8135.xml) ?

Does it possible to obtain/create  MC56F8135.xml ?

Thank's for your help

Edouard

Labels (1)
0 Kudos
Reply
1 Solution
2,533 Views
edouardmalot
Contributor II

Ok, the USB TAP was out of order.
With a new USB TAP it works well.

View solution in original post

0 Kudos
Reply
1 Reply
2,534 Views
edouardmalot
Contributor II

Ok, the USB TAP was out of order.
With a new USB TAP it works well.

0 Kudos
Reply