CodeWarrior for HCS12(X) Microcontrollers v5.2 Eval

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for HCS12(X) Microcontrollers v5.2 Eval

ソリューションへジャンプ
3,390件の閲覧回数
tnriley
Contributor III

I am looking for a downloadable  eval copy of CodeWarrior for HCS12(X) Microcontrollers v5.2. I have a non-networked development machine that requires installation from a DVD,etc. Please advise, Thanks, TIm

ラベル(1)
0 件の賞賛
返信
1 解決策
2,595件の閲覧回数
tnriley
Contributor III
0 件の賞賛
返信
3 返答(返信)
2,595件の閲覧回数
tnriley
Contributor III

pastedImage_1.png

0 件の賞賛
返信
2,595件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

in addition, this is evaluation CWs (include CW5.2) download link:

Evaluation Software|NXP 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,595件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Tim

You  can first download the installer in the PC which can connect to internet ,

then copy the installer package into U disk , then use it to install on the non-networked development machine .

Does this can help ?


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------