CodeWarrior for 68020 and 68030

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for 68020 and 68030

1,327 Views
jan_soller
Contributor I

i installed the CodeWarrior for 68k V 3.3.1 / 4.2.7 , but i think this is to new for my old CPUs, i can't find this CPUTypes as target.

i need one that supports the 68020 and 68030 CPU, there are a older Version available that supports this?   

i would like to build a hardware monitor with mc68901 DUART Controller, there are possibly libs avaible in a archive?

best regards, jan

0 Kudos
Reply
1 Reply

1,222 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

These two devices 68020 and 68030 have been discontinued since around 18 years ago. We are short of support these devices for both HW and SW.

I suggest you use 3rd party IDE if in need. for example

https://www.ghs.com/products/68k_development.html

http://www.cosmic-software.com/68k.php


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply