CodeWarrior V11.1 USB TAP lost communication issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior V11.1 USB TAP lost communication issue

4,198件の閲覧回数
mgwalker95
Contributor II

Hi,

I am connecting to the WCT-15W1CFFPD dev board using a USB TAP. When I program the WCT1013 after clicking the start button CodeWarrior says that "The debugger has lost communication on connection "wct1013PDdemo_FLASH_LDM_FSL USB TAP""

When I try to reestablish connection it cannot. 

Is there a way to fix this issue so that I can debug the wct1013 in real time? 

0 件の賞賛
返信
3 返答(返信)

4,186件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Michael,

Pls confirm if you use "wct1013PDdemo_FLASH_LDM_FSL USB TAP" or "wct1013PDdemo_FLASH_SDM_FSL USB TAP"

BR

XiangJun Rong

 

0 件の賞賛
返信

4,164件の閲覧回数
mgwalker95
Contributor II

Hi,

I am using "wct1013PDdemo_FLASH_LDM_FSL USB TAP" is this the correct configuration?

0 件の賞賛
返信

4,187件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Michael,

I have tried my MC56F84789 board, I can communicate with TWR-568400 board.

I suggest you try the following process so that we can confirm that the USBTAP device is okay.

1)after you connect the target board, sure that the USBTAP can be identified.

xiangjun_rong_0-1602473693181.png

2)after you download the code, check the ccs tools:

xiangjun_rong_1-1602473743908.png

3)If your USBTAP device has issue, pls consider the Multilink Universal device from the link, which supports the MWCT10xx family:

http://www.pemicro.com/

Hope it can help you

BR

XiangJun Rong

 

 

 

0 件の賞賛
返信