CodeWarrior V11.1 USB TAP lost communication issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior V11.1 USB TAP lost communication issue

4,128 次查看
mgwalker95
Contributor II

Hi,

I am connecting to the WCT-15W1CFFPD dev board using a USB TAP. When I program the WCT1013 after clicking the start button CodeWarrior says that "The debugger has lost communication on connection "wct1013PDdemo_FLASH_LDM_FSL USB TAP""

When I try to reestablish connection it cannot. 

Is there a way to fix this issue so that I can debug the wct1013 in real time? 

0 项奖励
回复
3 回复数

4,116 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Michael,

Pls confirm if you use "wct1013PDdemo_FLASH_LDM_FSL USB TAP" or "wct1013PDdemo_FLASH_SDM_FSL USB TAP"

BR

XiangJun Rong

 

0 项奖励
回复

4,094 次查看
mgwalker95
Contributor II

Hi,

I am using "wct1013PDdemo_FLASH_LDM_FSL USB TAP" is this the correct configuration?

0 项奖励
回复

4,117 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Michael,

I have tried my MC56F84789 board, I can communicate with TWR-568400 board.

I suggest you try the following process so that we can confirm that the USBTAP device is okay.

1)after you connect the target board, sure that the USBTAP can be identified.

xiangjun_rong_0-1602473693181.pngxiangjun_rong_0-1602473693181.png

2)after you download the code, check the ccs tools:

xiangjun_rong_1-1602473743908.pngxiangjun_rong_1-1602473743908.png

3)If your USBTAP device has issue, pls consider the Multilink Universal device from the link, which supports the MWCT10xx family:

http://www.pemicro.com/

Hope it can help you

BR

XiangJun Rong

 

 

 

0 项奖励
回复