CodeWarrior USB TAP for MPC5121YVY400B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior USB TAP for MPC5121YVY400B

3,296 Views
db_1008
Contributor I

1. We need to order code warrior 900-75115 Rev g. However, it seems the TAP is obsolete.  Can you please guide us with the proper TAP which can be used for the programming of debugging purpose of this Processor.

2. if its new TAP, we can order newer ones also. Please suggest

 

Thanks

DB

Labels (1)
0 Kudos
Reply
3 Replies

3,250 Views
vageeshpanditha
Contributor II

Hi Jun Zhang,

Please advise COP Cable needed for this MPC52xx/MPC51xx Mobile GT processor to be purchased along with BASE CW TAP.

Regards,

Vageesh K M

0 Kudos
Reply

3,235 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Thanks for the reminder.

0 Kudos
Reply

3,273 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI DB

The part number of USBTAP that support MPC5200 is CWH-UTP-PPCC-HE. However it is not manufactured now.

Its replacement is CWH-CTP-BASE-HE.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW_TAP

 

and the CWH-CTP-COP-YE:
 

 

However if you are using CodeWarrior for MobileGT v9.2, you need install CCS update. For details, please review this document:

http://cache.freescale.com/files/32bit/doc/app_note/AN4780.pdf

 

Have a nice day,

Jun Zhang

0 Kudos
Reply