CodeWarrior S12Z linker not acknowledged

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior S12Z linker not acknowledged

跳至解决方案
2,539 次查看
pierluigi_milos
Contributor I

Hi,

During the building, CodeWarrior (10.6) stops due to the following error:

 

'Invoking: S12Z Linker'
"C:/Freescale/CW MCU v10.6/MCU/S12lisa_Tools/Build_Tools/linker" -ArgFile"application.args" -O"application.elf"
""C:/Freescale/CW MCU v10.6/MCU/S12lisa_Tools/Build_Tools/linker"" non Š riconosciuto come comando interno o esterno, un programma eseguibile o un file batch.
mingw32-make: *** [LMU_L7E_CU.elf] Error 1

 

I supposed that the .dll of linker was corrupted but I tried to replaced it, getting it from another PC where CodeWarrior 10.6 is installed, and I did not resolve.

I can't find any solution to this problem. Can someone help me?

 

Thanks

Regard!

标记 (1)
0 项奖励
回复
1 解答
2,432 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Pierluigi,

Try to uninstall it, then reinstall.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,432 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Pierluigi Milosa ,

This error occur just on your specified project, or all projects ? How about a simple project ?

You mentioned you test on other PC, how about it ? If it can work well, please reinstall  CW on your PC.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,432 次查看
pierluigi_milos
Contributor I

Hi Alice_Yang,

this error occurs on all the projects. After this error have been occurred on one project, it has started to appear on all the projects, even those worked before.

The same projects on another PC work well.

Do you think I need to reinstall CW?

Thanks

0 项奖励
回复
2,433 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Pierluigi,

Try to uninstall it, then reinstall.

0 项奖励
回复
2,432 次查看
pierluigi_milos
Contributor I

Hi Alice_Yang,

uninstalling and reinstalling CW, the problem was solved.

Thanks for your help

Have a great day

0 项奖励
回复