CodeWarrior S12Z linker not acknowledged

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior S12Z linker not acknowledged

Jump to solution
2,533 Views
pierluigi_milos
Contributor I

Hi,

During the building, CodeWarrior (10.6) stops due to the following error:

 

'Invoking: S12Z Linker'
"C:/Freescale/CW MCU v10.6/MCU/S12lisa_Tools/Build_Tools/linker" -ArgFile"application.args" -O"application.elf"
""C:/Freescale/CW MCU v10.6/MCU/S12lisa_Tools/Build_Tools/linker"" non Š riconosciuto come comando interno o esterno, un programma eseguibile o un file batch.
mingw32-make: *** [LMU_L7E_CU.elf] Error 1

 

I supposed that the .dll of linker was corrupted but I tried to replaced it, getting it from another PC where CodeWarrior 10.6 is installed, and I did not resolve.

I can't find any solution to this problem. Can someone help me?

 

Thanks

Regard!

0 Kudos
Reply
1 Solution
2,426 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Pierluigi,

Try to uninstall it, then reinstall.

View solution in original post

0 Kudos
Reply
4 Replies
2,426 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Pierluigi Milosa ,

This error occur just on your specified project, or all projects ? How about a simple project ?

You mentioned you test on other PC, how about it ? If it can work well, please reinstall  CW on your PC.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,426 Views
pierluigi_milos
Contributor I

Hi Alice_Yang,

this error occurs on all the projects. After this error have been occurred on one project, it has started to appear on all the projects, even those worked before.

The same projects on another PC work well.

Do you think I need to reinstall CW?

Thanks

0 Kudos
Reply
2,427 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Pierluigi,

Try to uninstall it, then reinstall.

0 Kudos
Reply
2,426 Views
pierluigi_milos
Contributor I

Hi Alice_Yang,

uninstalling and reinstalling CW, the problem was solved.

Thanks for your help

Have a great day

0 Kudos
Reply