CodeWarrior Fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior Fail

1,358 Views
peterzheng
Contributor II

Hi,

 

I was using codewarrior for some bareboard project. It was working fine until just now. Now when I open codewarrior, when I click on the Debug Configuration, or Run Configuration. Nothing shows. I didn't make any changes. I tried to restart my system. restart the CodeWarrior. But it didn't work.

 

Should I reinstall the CodeWarrior? If so, how can I preserve all my projects and profiling results?

 

Regards,

Peter

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,291 Views
TICS_Fiona
NXP Employee
NXP Employee

Are you logging on Windows as Administrator?  Are you using Floating license?

Please delete .metadata folder of workspace of CW 10.x.

Then reopen the project in CodeWarrior, and click on 'Project' menu-> Clean to remove the old object file, and then rebuild the project. Is the problem fixed?


If not, please create a new bareboard project and test again.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply