CodeWarrior Fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior Fail

1,294件の閲覧回数
peterzheng
Contributor II

Hi,

 

I was using codewarrior for some bareboard project. It was working fine until just now. Now when I open codewarrior, when I click on the Debug Configuration, or Run Configuration. Nothing shows. I didn't make any changes. I tried to restart my system. restart the CodeWarrior. But it didn't work.

 

Should I reinstall the CodeWarrior? If so, how can I preserve all my projects and profiling results?

 

Regards,

Peter

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,227件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Are you logging on Windows as Administrator?  Are you using Floating license?

Please delete .metadata folder of workspace of CW 10.x.

Then reopen the project in CodeWarrior, and click on 'Project' menu-> Clean to remove the old object file, and then rebuild the project. Is the problem fixed?


If not, please create a new bareboard project and test again.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信