CodeWarrior Custom Board Support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior Custom Board Support

1,789 次查看
reedy
Contributor III

I am trying to find details about how to add a custom board to the list of supported boards in CodeWarrior 10.5.2. I found a document in PA\PA_Tools\CustomBoardSupportToolkit\Documentation that seems promising however it references files that don't exist (the only document that exists in PA\PA_Tools\CustomBoardSupportToolkit is the 1 pdf). Is there an example that shows the steps necessary to add a custom board to CodeWarrior?

标签 (1)
0 项奖励
回复
2 回复数

1,712 次查看
addiyi
NXP Employee
NXP Employee

The AppNote you refer is pretty old, and indeed is not updated. Serial projects are located under \PA\PA_Support\Serial\ and you can use a stationery project as starting project for your custom board.

Basically, to add support for your board you have to change the init file according with your board settings. 

Adrian

0 项奖励
回复

1,712 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Christian

Please refer to this thread for how to bring up a custom board.

https://community.nxp.com/message/817598

 

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复