CodeWarrior Custom Board Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior Custom Board Support

1,717件の閲覧回数
reedy
Contributor III

I am trying to find details about how to add a custom board to the list of supported boards in CodeWarrior 10.5.2. I found a document in PA\PA_Tools\CustomBoardSupportToolkit\Documentation that seems promising however it references files that don't exist (the only document that exists in PA\PA_Tools\CustomBoardSupportToolkit is the 1 pdf). Is there an example that shows the steps necessary to add a custom board to CodeWarrior?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,640件の閲覧回数
addiyi
NXP Employee
NXP Employee

The AppNote you refer is pretty old, and indeed is not updated. Serial projects are located under \PA\PA_Support\Serial\ and you can use a stationery project as starting project for your custom board.

Basically, to add support for your board you have to change the init file according with your board settings. 

Adrian

0 件の賞賛
返信

1,640件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Christian

Please refer to this thread for how to bring up a custom board.

https://community.nxp.com/message/817598

 

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信