CodeWarrior Compile link question(Error -1073741811)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior Compile link question(Error -1073741811)

3,380 次查看
DerekXiang
Contributor I

Hi, All,

      My Compile environment is CodeWarrior 11.1 + Updates3. Computer systerm is Windows10.

      Error information is the following:       

**** Build of configuration FLASH_SDM_LPM for project 56F81768_HBLLC ****

"D:\\Freescale\\CW MCU v11.1\\gnu\\bin\\mingw32-make" -j8 all
'Building target: 56F81768_HBLLC.elf'
'Executing target #25 56F81768_HBLLC.elf'
'Invoking: DSC Linker'
"D:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwld56800e" -o "56F81768_HBLLC.elf" @@"56F81768_HBLLC.args"
mingw32-make: *** [56F81768_HBLLC.elf] Error -1073741811

       I clean this project and re-compile it. The error information is same. Then I build a new default project, and compile it, but the error information is same yet (mingw32-make: *** [xxxxxxx.elf] Error -1073741811). Then I re-install codewarrior 11.1+update3, the error information is same.

      How to settle it?  Hope to your help. Thanks!

    

0 项奖励
回复
3 回复数

3,243 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Derek

Please let us know this problem is on one specific project or a common issue for all project? 

How can reproduce your issue?

Thanks,

Jun Zhang

0 项奖励
回复

3,231 次查看
DerekXiang
Contributor I

Hi, zhangJennie

      This is a sudden problem. After I re-installed codewarrior IDE, I can normally compile the project.

0 项奖励
回复

3,228 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Good to know. Thanks for the sharing.

0 项奖励
回复