CodeWarrior ARMv8 - not setting HWA_CGA_M2_CLK_SEL RCW bits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior ARMv8 - not setting HWA_CGA_M2_CLK_SEL RCW bits

ソリューションへジャンプ
2,767件の閲覧回数
Davisg
Contributor III

When using CodeWarrior ARMv8 to generate a binary RCW to use for NOR FLASH boot of an LS1043A processor, the QorIQ configuration tool is not setting the HWA_CGA_M2_CLK_SEL bits (509-511). These bits are always set to 000 no matter which option is selected in QorIQ configuration.

 

I know that u-boot will generate the RCW/PBL with checksum from cfg files, and include the generated RCW/PBL in the binary for SD card and NAND boot but u-boot does not have facilities to do the same for a NOR image. How can I generate an RCW/PBL with HWA_CGA_M2_CLK_SEL set correctly and checksum generated outside of the CodeWarrior QorIQ configuration tool? Or is there a fix to the QorIQ configuration tool in CoeWarrior ARMv8?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,652件の閲覧回数
addiyi
NXP Employee
NXP Employee

You need to update QCVS to latest version which is 4.7.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,652件の閲覧回数
addiyi
NXP Employee
NXP Employee

What QCVS version you are using?

Adrian

0 件の賞賛
返信
2,652件の閲覧回数
Davisg
Contributor III

CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA

(c) Freescale Semiconductor, Inc. 2014. All rights reserved.
Learn more about CodeWarrior at
http://www.freescale.com/codewarrior

Version: 11.2.0
Build Id: 160115

0 件の賞賛
返信
2,653件の閲覧回数
addiyi
NXP Employee
NXP Employee

You need to update QCVS to latest version which is 4.7.

0 件の賞賛
返信