Hello,
I am using CodeWarior v11.1
I am trying to compile Bootloader(s) for S12Z family provided by NXP
in Application notes AN4723 and/or AN5389.
Without any change of the provided Project example (AN5389) I am get this error:
"mingw32-make: *** [S12ZVL128_bootloader.elf] Error 1"
"Out of allocation space in segment SHADOW_ROM_S at address 0xFFFD86"
(When I change linker file just error message changes from SHADOW_ROM_S to ROM.)
I have tried all 3 Bootloaders for S12Z provided by NXP AN12086, AN4723 and AN5389 as is.
Any time have the same Error.
I have read and try any suggestions in the forum, but without success.
Any help would be greatly appreciated
Regards
Ivan