Code warrior error "Dispatch Debugger Events"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code warrior error "Dispatch Debugger Events"

3,014 Views
Aman786
Contributor II

Hi,

I am facing the error "An internal error occurred during "Dispatch Debugger Events".

Could you please help me to resolve the issue ?

 

 

Thanks

AmanScreenshot 2023-11-30 162010.pngScreenshot 2023-11-30 162010.png

Tags (1)
0 Kudos
Reply
3 Replies

2,989 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I see that you use CodeWarrior for MCU ver11.x tools, could you tell us the part number for example MC56F8367, MC56F82748 ...and debugger probe for example USBTAP or Multilink Universal device you are using?

BR

XiangJun Rong

0 Kudos
Reply

2,978 Views
Aman786
Contributor II

Hi XiangJun,

 

The controller used is MC56F83789 and the Multilink USB is used.

 

However the issue was resolved by deleting .metadat folder from the workspace.

 

I additionally request you to provide some guidance on Processor Expert Tool its installation and configuration along with user manual. It would be helpful since i am new to codewarrior.

 

 

Thanks

Aman

0 Kudos
Reply

2,950 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, the MC56F83xxx including MC56F83789  supports neither Processor Expert nor quick start, but supports SDK.

Pls download SDK package from the website:

https://mcuxpresso.nxp.com/en/welcome

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply