Code warrior does not recognize global structure variable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code warrior does not recognize global structure variable

2,759件の閲覧回数
jaehak9708
Contributor II

Hi,

I'm using code warrior IDE version 5.9.0 for MPC55xx/56xx. 
pastedImage_1.png

According to my preference setting, the global variables should be purple. 

I declared the struct variable such as , 

// aaa.h

struct _A

{

   uint8_t a:1;

   uint8_t b:1;

   uint8_t :6;

}

void floor(void);

#ifdef _aaa_h_

  struct _A a_struct;

#else

  extern struct _A a_struct;

#endif

// aaa.c

#include "aaa.h"

void floor(void)

{

  a_struct.a = 1;

}

I think that the struct variable 'a_struct' will be purple. But it doesn't. Its color is white (foreground).

There is no compile error. 

When I declare the struct variable in main.h and main.c, It works, 

But in other source, header files, It doesn't apply. 

Is It just a bug? 

ラベル(1)
2 返答(返信)

2,690件の閲覧回数
ErichStyger
Specialist I

Somewhat probably unrelated, but:

You have this:

#ifdef _aaa_h_

  struct _A a_struct;

#else

  extern struct _A a_struct;

#endif

which is very unusual and even very dangerous: you never should have variable definitions in header files except you know exactly what you are doing. Because depending on that define and potentially include orders you will have multiple definitions. What you really should have is

extern struct _A a_struct;

in aaa.h

and

struct _A a_struct;

in aaa.c.

As a positive side effect, I guess your coloring thing will go away too.

I hope this helps,

Erich

2,690件の閲覧回数
jaehak9708
Contributor II

You are right, Thank you :smileyhappy:

Regards, 

Jaehak Kim