Code warrior 4.02

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code warrior 4.02

1,628 Views
dipikakamat
Contributor I

Hi ,

I am using Code warrior 4.02 IDE to compile a code which was previously built using the same IDE for DSP56F805 MCU.

I want to know how to open a previously created project,compile it and generate the .elf file?

Can anybody help me in this ?

Thanks in advance.

Labels (1)
0 Kudos
Reply
3 Replies

1,552 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Dipika

By default, the help documents for CodeWarrior is placed under CodeWarrior folder, usually is:

C:\Program Files\Freescale(Motorola)\CodeWarrior\Help

To create a new project in CodeWarrior, please click on File Menu ->New->DSP56800x EABI Stationery. 

I have no IDE 4.02, but the method should be same. 

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,551 Views
dipikakamat
Contributor I

Hi Fiona,

PFA.

I am getting this SDK related error when i try to generate the .elf

file.Please help me resolve this error.

Thanks and Regards,

Dipika Kamat

Assistant System Engineer

Tata Consultancy Services

STP-Unit,House No.65/A-5,

NEAR CIVIL & CRIMINAL COURT

ALTINHO, Mapusa- Goa,

India

Mailto: kamat.dipika@tcs.com.

0 Kudos
Reply

1,551 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Dipika

If your source code does not use SDK, please create your project by selecting ‘Dsp56800 EABI Stationery’ instead of ‘Embedded SDK Stationery’.

Best Regards

Fiona Kuang

TIC - Technical Information Center

0 Kudos
Reply