Code warrior 4.02

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code warrior 4.02

2,566件の閲覧回数
dipikakamat
Contributor I

Hi ,

I am using Code warrior 4.02 IDE to compile a code which was previously built using the same IDE for DSP56F805 MCU.

I want to know how to open a previously created project,compile it and generate the .elf file?

Can anybody help me in this ?

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,490件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Dipika

By default, the help documents for CodeWarrior is placed under CodeWarrior folder, usually is:

C:\Program Files\Freescale(Motorola)\CodeWarrior\Help

To create a new project in CodeWarrior, please click on File Menu ->New->DSP56800x EABI Stationery. 

I have no IDE 4.02, but the method should be same. 

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,489件の閲覧回数
dipikakamat
Contributor I

Hi Fiona,

PFA.

I am getting this SDK related error when i try to generate the .elf

file.Please help me resolve this error.

Thanks and Regards,

Dipika Kamat

Assistant System Engineer

Tata Consultancy Services

STP-Unit,House No.65/A-5,

NEAR CIVIL & CRIMINAL COURT

ALTINHO, Mapusa- Goa,

India

Mailto: [email protected].

0 件の賞賛
返信

2,489件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Dipika

If your source code does not use SDK, please create your project by selecting ‘Dsp56800 EABI Stationery’ instead of ‘Embedded SDK Stationery’.

Best Regards

Fiona Kuang

TIC - Technical Information Center

0 件の賞賛
返信