Code warrier upgarde

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code warrier upgarde

2,305 Views
charudattaingal
Contributor IV

Dear Team

 

I upgrade the code  warier 10.6 it got upgraded successful.

At the start up one pop up came PE debugger Firmware is out of date then I upgrade the PE debugger firmware.

Now PE debugger is not working fine It is getting restart frequently.

Requesting help for the same.

Labels (1)
0 Kudos
Reply
3 Replies

2,147 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

what P&E tool do you work with?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,147 Views
charudattaingal
Contributor IV

Hi Jennie Zhang

I am using PE Micro Multilink universal Rev c and CodeWarrior Version: 10.6.4 Build Id:150416

Thanks & Regards,

Charudatta

0 Kudos
Reply

2,147 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Charudatta,

please download and update the firmware with latest firmware update utility, up-to-date firmware:

http://www.pemicro.com/downloads/main_downloads_temp/201603080313261325454/multilink_universal_insta...

can this help you?
Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply