Code Warrior USB Tap "Device Protection Error" for IN28F640J3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior USB Tap "Device Protection Error" for IN28F640J3

1,915 Views
mehmetalinbay
Contributor I

Hi everyone;

We've custom board with MCP8548 & JS28F640J3F75A NOR flash. We're using another debug probe to download binaries but we wanted to use Code Warrior USB Tap.

We configüred flash programmer IN28F640J3 as NOR Flash but in some sectors we're getting "Device Protection Error" from CodeWarrior

Error seems like this:

* 0x00000 ~ 0x1FFFF --> Download & verify OK

* 0x20000 ~ 0x3FFFF --> Protection Error

* 0x40000 ~ 0x5FFFF --> Download & verify OK

* 0x60000 ~ 0x7FFFF --> Protection Error

So basically it seems one sector Ok, other sector Protection Error.

I'm also sending our debugger log as attachment

Thanks   

0 Kudos
Reply
1 Reply

1,909 Views
yipingwang
NXP TechSupport
NXP TechSupport

1. In PA Flash Programmer Task panel, target RAM  configuration, please specify the size of the RAM as 0x80000.

2. Please use initialization file 8548CDS_init_sram.tcl to avoid to configure DDR memory.

3. In CodeWarrior initialization file, please modify "configure Local Bus memory controller" section (BR0, OR0) according to your NOR flash. Please refer to MPC8548 reference manual for detailed description about register BR0 and OR0.

0 Kudos
Reply