Code Warrior Burning new U-boot Execute command is not enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior Burning new U-boot Execute command is not enabled

Jump to solution
5,410 Views
yusufalti4444
Contributor I

Hi NXP,

I am trying to burn new U-boot on T1042 D4 RDB as described in QorIQ SDK V2.0 - 1703 (Chapter 5) using Code Warrior for T1042. It's the latest Code Warrior Development Studio. I created a sample BareBoard project for T1042 D4 RDB. 

I created a new Target Task as described in documentation but Execute command on Target Task window is not getting enabled. I can run project and I am having console logs.  Documentation says it gets enabled when the debugger is online. My Code Warrior Tab is working. TX/RX led is blinking green and RUN/PAUSE led is lighting red.

I attached Screenshots for more information. Console logs and disabled Execute button can be seen in these screenshots.

What is the reason of this situation, how can I solve it ?

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
5,313 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ahmet Demir,

For flash programming, please refer to the step by step document Flash Programmer for CodeWarrior Power Architecture

1. First please create a board project with Download/Connect SRAM launch configuration.

2. Please import XML task template file for T1042D4 RDB, and add flash programing action in "PA Flash Programmer Task". .

3. Please connect to the target board from Run->Debug configuration -><project>-core00_SRAM_T1040_Connect->Debug, then the "Execute" button is available.

4. Please click "Execute" button to perform flash programming.

Thanks,

Yiping

 

View solution in original post

0 Kudos
Reply
1 Reply
5,314 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ahmet Demir,

For flash programming, please refer to the step by step document Flash Programmer for CodeWarrior Power Architecture

1. First please create a board project with Download/Connect SRAM launch configuration.

2. Please import XML task template file for T1042D4 RDB, and add flash programing action in "PA Flash Programmer Task". .

3. Please connect to the target board from Run->Debug configuration -><project>-core00_SRAM_T1040_Connect->Debug, then the "Execute" button is available.

4. Please click "Execute" button to perform flash programming.

Thanks,

Yiping

 

0 Kudos
Reply