Client open CW2.10 IDE error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Client open CW2.10 IDE error

3,053 Views
leolv
Contributor II

Our company  have purchased CW Perpetual-Floating version and received the U disk. then i setup the environment following the spec "FLOATING LICENSE
INSTALLATION FOR WINDOWS".

when i try to open CW2.10 from client, it report error "no valid license key was found", more information please refer to attachment. Who can help to setup this?

0 Kudos
Reply
4 Replies

2,993 Views
leolv
Contributor II

Client can use the server license file now, but if the network is not ok, client will stop working immediately. Is that normal? 

0 Kudos
Reply

2,987 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

yes,it's normal. if using floating license we must make sure local network well.

Have a nice day,

Jun Zhang

 

0 Kudos
Reply

1,829 Views
leolv
Contributor II

If a computer that is not on the same local area network as the server wants to access and use the CW floating license on our server, how can it be done

Tags (1)
0 Kudos
Reply

3,028 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI leolv ,.

The error message means your CW doesn't find correct license on server.

First ping server from client, make sure network  ok. 

then change license file

FROM: this_host
TO: Your license server's host IP address, or your license server's host name

make sure the license.dat file is installed under both server FlexIM folder and client CW install folder.

Restart computer after everything set up.

If still has problem, create a private case to NXP license support team, with you license file. As it is related with personal asset, we can't post ti to public comunity.

Have a nice day,

Jennie

0 Kudos
Reply