Does Code Warrior V2.10 for MPC5554 support C99 Standard?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does Code Warrior V2.10 for MPC5554 support C99 Standard?

1,204 Views
fangfang1
Contributor I

Does Code Warrior V2.10 for MPC5554 support C99 Standard?

Tags (1)
0 Kudos
Reply
1 Reply

1,197 Views
stanish
NXP Employee
NXP Employee

Hi, 

CodeWarrior for MPC55xx v2.10 does support C99 extension (ISO/IEC 9899-1999)

It could be enabled in project settings (ALT+F7) -> C/C++ Language

Or ther is a command line option "-dialect c99"

stanish_0-1755903966841.png

 

Hope it helps,

Stan

 

 

0 Kudos
Reply