Cannot import Kinetis_Exsamples

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Cannot import Kinetis_Exsamples

跳至解决方案
2,266 次查看
tadahirotakase
Contributor II

I cannot import Kinetis_Examples\KE\GPIO_demo. My CW version is 10.6.

I imported Existing Projects into Workspace.

Projects: GPIO_demo (c\Freescale\CW MCU v10.6\MCU\CodeWarrior_Examples\Kinetis_Examples\KE\build\cw\ke02\GPIO_demo).

Clean and Build. Then Errors (1 items). Mingw32-make: *** No rule to make target….

Question1: Why?

Question2: I cannot view GPIO_demo.c. Error retrieving content description for resource GPIO_demo.c. Why?

Please teach me answers.

Best Regard.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,010 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Tadahiro Takase:

Those example projects have relative include paths. It seems you are copying the project instead of importing the original, so the relative paths are not valid anymore.

To solve the problem do this:

1) Delete the project from your workspace:

Delete_project.png

2) Import the project again, but uncheck the box "Copy projects into workspace":

Import_project.png

Now you can build with no errors and also you can open GPIO_demo.c.

Regards!,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,011 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Tadahiro Takase:

Those example projects have relative include paths. It seems you are copying the project instead of importing the original, so the relative paths are not valid anymore.

To solve the problem do this:

1) Delete the project from your workspace:

Delete_project.png

2) Import the project again, but uncheck the box "Copy projects into workspace":

Import_project.png

Now you can build with no errors and also you can open GPIO_demo.c.

Regards!,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复