Cannot import Kinetis_Exsamples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot import Kinetis_Exsamples

ソリューションへジャンプ
2,369件の閲覧回数
tadahirotakase
Contributor II

I cannot import Kinetis_Examples\KE\GPIO_demo. My CW version is 10.6.

I imported Existing Projects into Workspace.

Projects: GPIO_demo (c\Freescale\CW MCU v10.6\MCU\CodeWarrior_Examples\Kinetis_Examples\KE\build\cw\ke02\GPIO_demo).

Clean and Build. Then Errors (1 items). Mingw32-make: *** No rule to make target….

Question1: Why?

Question2: I cannot view GPIO_demo.c. Error retrieving content description for resource GPIO_demo.c. Why?

Please teach me answers.

Best Regard.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,113件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Tadahiro Takase:

Those example projects have relative include paths. It seems you are copying the project instead of importing the original, so the relative paths are not valid anymore.

To solve the problem do this:

1) Delete the project from your workspace:

Delete_project.png

2) Import the project again, but uncheck the box "Copy projects into workspace":

Import_project.png

Now you can build with no errors and also you can open GPIO_demo.c.

Regards!,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,113件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Tadahiro Takase:

Those example projects have relative include paths. It seems you are copying the project instead of importing the original, so the relative paths are not valid anymore.

To solve the problem do this:

1) Delete the project from your workspace:

Delete_project.png

2) Import the project again, but uncheck the box "Copy projects into workspace":

Import_project.png

Now you can build with no errors and also you can open GPIO_demo.c.

Regards!,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信