Can't step through code using PE Micro Multilink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't step through code using PE Micro Multilink

2,100件の閲覧回数
usr4691
Contributor I

I built an .ELF file using Code Warrior for MPC55XX and tried to debug it using the PE Micro USB MULTI-LINK Interface. When pressing the bebug button I get the message 'Can't read symbolocs for target <generator.elf>'. My question is how do I get the PE Micro Multilink USB Interface device to step through the elf code loaded onto my MPC5674 board.

ラベル(1)
タグ(5)
0 件の賞賛
返信
2 返答(返信)

1,970件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Barton,

There are several versions of Multilink supporting MPC5xxx:

    - USB Qorivva Multilink -> http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320021

    - USB Multilink Universal  -> http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137

    - USB Multilink Universal FX -> P&E Microcomputer Systems - USB Multilink Universal FX - USB Multilink Universal FX All-In-One Devel...

To check the configuration I recommend you to:

      - create a sample project with the wizard with your configuration,

      - build the project,

      - launch the debugger.

The application should be load and you should be able to debug it.


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,970件の閲覧回数
usr4691
Contributor I

The Code Warrior version is 2.7.

0 件の賞賛
返信