Can't secure device. MK20DN128VLF5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't secure device. MK20DN128VLF5

ソリューションへジャンプ
3,463件の閲覧回数
alexx_88
Contributor III

Hello all,

 

We've finalized our first project with the Kinetis line and now is time to go into production, but ran into problems with securing the device:

 

1. First of all, even after enabling security in Processor Expert, the flash configuration byte was set to:

/* NV_FSEC: KEYEN=1,MEEN=3,FSLACC=1,SEC=3 */     0x77U,

 

which wasn't correctly written in flash. We've got around that by changing the SEC bits from 10 to 00, an issue described in another thread on this forum.

 

2. After fixing the first problem, we've run into another error, this time related to the configuration file used by Segger JLink.

 

10933_10933.pngsecure_problem.png

 

CodeWarrior Version: 10.5 (free edition)

JLink Version: 4.74

 

Has anybody else run into this sort of issue before?

 

Cheers,

Alex

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
3,271件の閲覧回数
handychandra
Contributor III

I was using flash programmer in code warrior 10.5 trial and it works fine. It was "flash file to target".

My debugger is j-link edu

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,271件の閲覧回数
alexx_88
Contributor III

Thanks, that worked!

I was under the impression that I tried it and didn't work.

0 件の賞賛
返信
3,272件の閲覧回数
handychandra
Contributor III

I was using flash programmer in code warrior 10.5 trial and it works fine. It was "flash file to target".

My debugger is j-link edu

0 件の賞賛
返信