Can't find the SDA connection on Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't find the SDA connection on Flash

1,788 Views
shiroe0329
Contributor I

Hello everyone

In my case.

I can find my PEMicro OpenSDA Debug Drive in Jungo also can debug.

But when I want to flash the target to my board(KEAZN64).

It can't find the connection and when I create a new connection.

It will get a storage error and can't get the target program to my board.

Can anyone help me to slove this problem?

Thanks a lot!!

Labels (1)
0 Kudos
Reply
2 Replies

1,720 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

From your screenshot , it seems you use the Flash File to Target function,

there is a introduce about it  of the attachment :

3.12 Flash File to Target

If you still have question , please show the steps one by one about how do you

configure it,  then i can reproduce it on my side .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,720 Views
shiroe0329
Contributor I

Thanks Alice

I found the problem finally

Cauz I use Debug then forget to stop it

That's why I can't use Flash the target file

Thanks for your reply again!

0 Kudos
Reply