CWH-UTP-PPCD-HE DPI TO JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CWH-UTP-PPCD-HE DPI TO JTAG

4,505 Views
2007031026
Contributor II

Hi! I have got a problem that I bought  a wrong USB Tap.The part number is CWH-UTP-PPCD-HE which is DPI interface.But the debug interfce that I need is JTAG.Now,Can you offer a  correct part number of the JTAG interface Code Warrior USB Tap for debuging PowerPC processor T2080 and MPC8640D,or is there some file that introduce the simulator's ordering information? If there is a convertor can change the DPI to JTAG interface? Or is there someone could change this simulator to JTAG interface? And can I do some change to the CWH-UTP-PPCD-HE USB Tap to make it to JTAG interface as some file's guide? And is there some suggestion? Thanks!

0 Kudos
Reply
4 Replies

4,316 Views
Pavel
NXP Employee
NXP Employee

It looks lie that this request should be addressed to your seller.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,316 Views
2007031026
Contributor II

Dear Pavel Chubakov,

    Thanks for your reply!

    Have a great day!

0 Kudos
Reply

4,314 Views
Pavel
NXP Employee
NXP Employee

Look at the following document:

https://www.nxp.com/webapp/Download?colCode=950-00126&location=null&fsrch=1&sr=2&pageNum=1&Parent_no...

 

This document is available in the attachment.

The USBTAP JTAG (PQ II/III) CWH-UTP-PPCC-HE is needed for the T2080 and MPC8640D.

 

NXP offers CodeWarrior 10.5.1 for the T2080:

http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-to...

 

This CodeWarrior uses CodeWarrior TAP for software developing:

http://www.nxp.com/products/microcontrollers-and-processors/more-processors/dsp-dsc/codewarrior-tap:...

 

CodeWarrior TAP also can be used for software developing and programming under CodeWarrior 8.8 for the MPC8641D.

 

This CodeWarrior TAP uses the following tip for connection to JTAG/COP interface of the T2080 and MPC8641D.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,314 Views
2007031026
Contributor II

Dear Pavel Chubakov,

    Thanks for your reply!

    Is there any way could change the CWH-UTP-PPCD-HE to CWH-UTP-PPCC-HE? 

    Thanks!

0 Kudos
Reply