CW11 for S12 "internal compiler error"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW11 for S12 "internal compiler error"

1,055 Views
mnovaro
Contributor I

I get the following compiler error

 

..\BSW\KERNEL\MCAL_S12x\mcu\Mcu.c:211: internal compiler error (report to

..\BSW\KERNEL\MCAL_S12x\mcu\Mcu.c:211: <cw_bug@freescale.com>)

..\BSW\KERNEL\MCAL_S12x\mcu\Mcu.c:211: while executing in file 'Coloring.c'

..\BSW\KERNEL\MCAL_S12x\mcu\Mcu.c:211: line: 698

..\BSW\KERNEL\MCAL_S12x\mcu\Mcu.c:211: (compiling 'Mcu_InitClock' in 'Mcu.c')

 

Trying to compile the a function for the S12 target. I’m using the following compiler version (mwccs12lisa):

 

CodeWarrior C/C++ for S12/L-ISA.

Copyright (c) 2017, Freescale Semiconductor, Inc

All rights reserved.

Version 5.0.44 (build 17292)

Runtime Built: Oct 20 2017 21:44:00

 

Using the default options provided by the project wizard (currently, no optimizations are on).

 

Any indication from your side about the cause of the error, and a possible workaround or fix, would be very welcome.

This issue is quite urgent for our development.

 

Thank you in advance, and best regards.

Marco

0 Kudos
Reply
1 Reply

926 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Marco,

To investigate your problem correctly and efficiently, please provide us the follows:
1.    your CW version: Start the IDE and click on Help | About CodeWarrior Development Studio. Send me the version and build id.
2.    send the entire sample code folder(include .project, prm,c...) in zip format to me. so that i can test it on my side directly.
3.      error screenshot.

Thanks for your cooperation.

Best Regards

Jennie Zhang

0 Kudos
Reply