CW11.1 license error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW11.1 license error

Jump to solution
2,176 Views
leolv
Contributor II

leolv_1-1735634072618.png

 
Installed Products:
 - CodeWarrior for MCU
Version: 11.1
Build Id:181224

 

#above is version and license information

#but when i open the IDE it always report errors below

leolv_2-1735634218409.png

how to fix this issue

In addition i am not sure where i should place my licesne.dat in client side.

 

 

0 Kudos
Reply
1 Solution
2,148 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @leolv ,

Thanks for your post. From your picture, it shows that your license.dat is in the right place and has been activated successfully. There's no problem. Regarding the log "CDE: no license found, using Community Edition License", it is not an error log but a normal one, and the appearance of this message will not affect the normal use of CodeWarrior. CDE means the Component Development Environment. You can refer to the link below for more details.

Solved: What tool do I kneed for Component Development? - NXP Community

In short, this log is not an error and won't affect your use. 

Hope it can help you. 

BRs,

Celeste

---------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
---------------------------------------------------------------------------------------------------

 

View solution in original post

1 Reply
2,148 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @leolv ,

Thanks for your post. From your picture, it shows that your license.dat is in the right place and has been activated successfully. There's no problem. Regarding the log "CDE: no license found, using Community Edition License", it is not an error log but a normal one, and the appearance of this message will not affect the normal use of CodeWarrior. CDE means the Component Development Environment. You can refer to the link below for more details.

Solved: What tool do I kneed for Component Development? - NXP Community

In short, this log is not an error and won't affect your use. 

Hope it can help you. 

BRs,

Celeste

---------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
---------------------------------------------------------------------------------------------------