CW10.6 import project become error.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW10.6 import project become error.

2,459 次查看
wanghaha
Contributor I

This is the error:"Description Resource Path Location Type
mingw32-make: *** No rule to make target `E:/CW10.6/TPMS_FXTH87_LF_RF_Communication_CW10_rev3/FXTH87xx11_CW10_2015_9_APP_AND_BOOT/Sources/app_source/app_global_vars.c', needed by `Sources/app_global_vars_c.obj'. Stop. FXTH87xx11_CW10_2015_9_APP C/C++ Problem."

And I used "Clean Project",it doesn't work. I don't know how to do,hope some one can help me.Thanks.

0 项奖励
回复
4 回复数

2,366 次查看
Carlos_Mendoza
NXP Employee
NXP Employee


Hi Wang,

Could you tell us which example project are you trying to import?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复

2,366 次查看
wanghaha
Contributor I

1493795359(1).png

0 项奖励
回复

2,366 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Wang,

It seems like there is a problem in the file app_global_vars.c, could you post the console information? it will give us more information on what could be causing the problem.

I also noticed that the project seems to be based on the below reference project, maybe you can use this working project as reference and add the extra files from your project:

http://www.nxp.com/assets/downloads/data/en/lab-test-software/TPMS-FXTH87-LF-RF-Communication-CW10.z... 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复

2,366 次查看
wanghaha
Contributor I

Hi Carlos,

I was adding the engineering steps to the document, another project "Import Project", then "Clean Project" and then "Build" can be successful but this one project does not work.I used the project hand in someone else, and now he has left. Before it can be opened and build on his computer but can not be build on my computer.Is not configured a problem?

Thank you very much.

0 项奖励
回复