CW for QorIQ 11.2.0 is not updated

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW for QorIQ 11.2.0 is not updated

2,513 Views
maxprakapovich
Contributor I

Hi ,

I'm clicking on Check for Update, responds No updates were found but there is a version 11.2.3.

I assume that there is no connection to update server. What could be the problem? What is there a way to upgrade?

Thanks!


 
0 Kudos
Reply
4 Replies

2,278 Views
addiyi
NXP Employee
NXP Employee

The Check for Updates works fine (maybe there was some network issues).

pastedImage_1.png

But, note that using Check for Updates, the updates is not performed fine. You have to use Help > Install New Software and choose ARMv8 Eclipse Update Site - http://freescale.com/lgfiles/updates/Eclipse/11.2.0/com.freescale.armv8_win as Work with update site.

Adrian

0 Kudos
Reply

2,278 Views
maxprakapovich
Contributor I

Thanks for response.
I forget tell my platform is Linux.

Link for Windows:

Screenshot from 2017-03-06 14_17_13.png

Link for Linux:
Screenshot from 2017-03-06 14_15_34.png

0 Kudos
Reply

2,278 Views
addiyi
NXP Employee
NXP Employee

Update site was fixed.

Adrian

0 Kudos
Reply

2,278 Views
addiyi
NXP Employee
NXP Employee

Indeed there is a problem. Thanks for point it out. It will be fixed is short time. Meanwhile, you can contact your FAE representative for offline package.

Adrian

0 Kudos
Reply