CW connect DEVKIT-S12XE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW connect DEVKIT-S12XE

2,665件の閲覧回数
edison_wu76
Contributor I

Hi Sir,

I got the error message when I try to debug code on the DEVKIT-S12XE.

Could you help to the issue ?

Edi.

image.png

image.png

0 件の賞賛
返信
4 返答(返信)

2,532件の閲覧回数
kef2
Senior Contributor V

Edison,

sounds like you have secured your S12XE. It could be caused by ECC failure in flash security phrase. Security may get engaged if you use CodeWarrior to download project, which specifies any of P-flash protection byte at 0x7F_FF0C, EEE protection byte, flash nonvolatile byte, or flash security byte. If you do specify any of these, then you need to add to your connection xxx_Preload.cmd this line

FLASH NOUNSECURE

it will solve issue of double flash security phrase programming (which causes ECC failure and forces security enable).

I don't know does DEVKIT-S12XE have P&E Multilink on board or something else. If Multilink then you may download Unsecure12 utility from pemicro.com.

Edward

0 件の賞賛
返信

2,532件の閲覧回数
edison_wu76
Contributor I

Hi Edward,

thanks for your reply.

It's ok. The EVB is secure at debug mode.

Edison.

0 件の賞賛
返信

2,532件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello edison,

Sorry I'm afraid  I can't get your picture, it just shows like below, also when click it , there is nothing.

pastedImage_1.png

Could you please just paste it on here or attached it .

BTW, which CW you used ?

Thanks.

BR

Alice

0 件の賞賛
返信

2,532件の閲覧回数
edison_wu76
Contributor I

Hi Alice,

The problem is solved.

THX.

Edison.

0 件の賞賛
返信