CW TAP with windows 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW TAP with windows 10

1,419 Views
rakshasrinivas
Contributor I

I am using CW TAP to connect to my system with P2020. I connect via USB from my windows 10 system. CW for PA version 10.5.1. Should i update the CW TAP firmware or my drivers?

Labels (1)
0 Kudos
Reply
1 Reply

1,245 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Raksha Srinivas,

As usual, no need to update CodeWarrior TAP firmware, when install CodeWarrior 10.5.1, CCS USB driver for CodeWarrior TAP has already been installed automatically.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply