How do I configure DDRv tool to connect to a target with other devices present in the JTAG chain?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I configure DDRv tool to connect to a target with other devices present in the JTAG chain?

1,708件の閲覧回数
tiagobrusamarel
Contributor V

Hello.

 

How do I configure the DDRv tool connection to access a target when other devices are present in the JTAG chain?

 

Regards.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,578件の閲覧回数
addiyi
NXP Employee
NXP Employee

For multiple device on chain support in QCVS please contact NXP support.

Adrian

0 件の賞賛
返信

1,578件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Unlike CodeWarrior, DDRv tool doesn't provide this function.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信